Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79194members
343734posts

ups keeps running in battery power

Solved
mani_firebolt_apc
Cadet
0 Likes
1
92

ups keeps running in battery power

This was originally posted on APC forums on 12/26/2011


i have a apc back-ups 600 and when there s a fluctuation it switches to battery mode and keeps beeping when the fluctuation settles the ups stays in battery mode till it switches off even after trying to unplug and plugging it back to the main this happens what should i do??

Tags (1)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
92

Re: ups keeps running in battery power

This reply was originally posted by Jonathan on APC forums on 12/27/2011


Hi Mani,

Were you able to measure the incoming voltage that is being fed into the UPS after the fluctuation? Also, when the fluctuation was over have you ever attempted turning the UPS off and on again? How about the frequency distortion? Are we sure that a good frequency is being fed as well?

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
93

Re: ups keeps running in battery power

This reply was originally posted by Jonathan on APC forums on 12/27/2011


Hi Mani,

Were you able to measure the incoming voltage that is being fed into the UPS after the fluctuation? Also, when the fluctuation was over have you ever attempted turning the UPS off and on again? How about the frequency distortion? Are we sure that a good frequency is being fed as well?