Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79338members
344031posts

Windows XP Update SP2 to SP3 Update Shutdown Powerchute.exe?

edge_apc
Cadet
0 Likes
0
45

Windows XP Update SP2 to SP3 Update Shutdown Powerchute.exe?

This was originally posted on APC forums on 8/5/2010


I am going to update Win XP to SP3 and part of the Microsoft instructions are to shut down all programs during the update installation.. Should I shutdown powerchute.exe from task manager and is there a way to stop powerchute from starting on boot up? I would like the first boot after the update with only necessary programs running and then will reconfigure. I have Winpatrol which can modify the Win startup programs. I am running Powerchute version 2.0 with a ES BE350R, is there a later version that is compatible with SP3? Thanks.