Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 12:54 AM
This was originally posted on APC forums on 5/27/2009
I've read through some of the posts here related to running PCPE on Server 2003 without finding this specific question.
I realize this is NOT a supported configuration, but I have a BE750G and can only use PCPE.
So if I'm going to install PCPE on Server 2003, which is the best version to use (2.0, 2.1.1 or 2.2) ??
Thanx in advance,
e
Posted: 2021-06-29 12:55 AM
This was originally posted on APC forums on 5/28/2009
Which version of .NET does 2.2 require ??
Posted: 2021-06-29 12:54 AM
This reply was originally posted by Angela on APC forums on 5/27/2009
as long as you take the risks into account, i would base it on XP - so I would use 2.0.
on XP, you can use Vista only version of 2.2 but .NET framework needs to be on your system for it to work. so if you dont want to tinker around, i can say that 2.0 works no problem.
Posted: 2021-06-29 12:54 AM
This reply was originally posted by Angela on APC forums on 5/28/2009
oh sorry! .NET framework 2.0
Posted: 2021-06-29 12:54 AM
This was originally posted on APC forums on 6/30/2009
IPAW,
So, if I have dot-Net v3.5 installed on my server and clients, I can now upgrade to PCPE v2.2?
Thanks,
Duncan
Posted: 2021-06-29 12:54 AM
This reply was originally posted by Angela on APC forums on 6/30/2009
yes i believe so.
Posted: 2021-06-29 12:54 AM
This was originally posted on APC forums on 7/1/2009
Duncan,
If you just want your Windows 2003 Server to shutdown gracefully in the event of low battery condition when the BE750G is on battery mode, you can also configure the USB native support(Control Panel-->Power Option) which is same as the PCPE graceful shutdown functionality. You would need to uninstall the PCPE software from your server in order for the Windows native support to enable.
Posted: 2021-06-29 12:55 AM
This was originally posted on APC forums on 3/14/2011
Techie,
I so missed this share. Sorry!
FWIW, FirePuppy started this thread; I jumped in-stream because I had the same question.
Situation may be academic now because PCPE V3.0 has been tried; and, does NOT work!
In any case, I do NOT allow my clients/servers to power themselves down via any SW program.
When I have a home power event and the lights go out. I manually power my server and clients OFF.
When the lights come back on, I power all the toys back on again. Works for me.
Thanks,
Duncan
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.