Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79290members
343968posts

Unit turns on, gives green light for 5-10 seconds, and then craps out.

Solved
nicechiguy_apc
Crewman
Crewman
0 Likes
1
80

Unit turns on, gives green light for 5-10 seconds, and then craps out.

This was originally posted on APC forums on 9/26/2010


I have a BACK-UPS ES 500. This issue does not seem to be addressed in the troubleshooting section of the manual.

I plug in the unit, I get the one short beep and the green light just turns on for 5-10 seconds. With no devices plugged in, the unit's green LCD just turns off and the unit sounds an incessant siren (I would not call it beeps because there are no pauses in the sound, nor does the sound change).

Any suggestions would be appreciated.


Accepted Solutions
nicechiguy_apc
Crewman
Crewman
0 Likes
0
80

Re: Unit turns on, gives green light for 5-10 seconds, and then craps out.

This was originally posted on APC forums on 9/28/2010


The unit has been installed for a while and without incident until just recently.

The exact model number and first six of the serial are: BE500U & JB0233

See Answer In Context

1 Reply 1
nicechiguy_apc
Crewman
Crewman
0 Likes
0
81

Re: Unit turns on, gives green light for 5-10 seconds, and then craps out.

This was originally posted on APC forums on 9/28/2010


The unit has been installed for a while and without incident until just recently.

The exact model number and first six of the serial are: BE500U & JB0233