Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 11:26 PM
This question was originally posted by E. on APC forums on 9/16/2013
My UTS6H is scheduled to be wired in next week, covering my key circuits: sump pump, furnance, well pump, refrigerator and a lighting circuit or two. It got me thinking, is the UTS designed so that if it fails, the circuits remain on utility power? In other words, in the 99.9% of the time when utility power is fine, but the circuit board were to fail, is the design such that circuits wouldn't be failed over on to the backup source?
Posted: 2021-06-29 11:26 PM
This reply was originally posted by E. on APC forums on 9/20/2013
I think I see from the circuit diagram how they would work to bypass a circuit, but I won't say it here in case I'm wrong.
I think it would be helpful to have something authoritative. After all, these are critical circuits I'm moving onto an electronic device with, no offense, a two year warranty, and if I understand you, if it fails my critical circuits fail.
Also, kudos to the engineers for providing a simple way to restore functionality if the panel fails.
Posted: 2021-06-29 11:26 PM
This reply was originally posted by Angela on APC forums on 9/16/2013
If the panel were to fail, you would have to manually bypass the failed circuit by placing the included faston in line with the Input and Output of the designated circuit.
Posted: 2021-06-29 11:26 PM
This reply was originally posted by E. on APC forums on 9/17/2013
Thanks. Is this documented somewhere? I couldn't find it in the operations and installation manuals.
Posted: 2021-06-29 11:26 PM
This reply was originally posted by Angela on APC forums on 9/17/2013
I only found it here -> http://www.apcmedia.com/salestools/KBOK-74JRFQ/KBOK-74JRFQ_R3_EN.pdf in the inventory section where it lists fastons. No good details on the purpose of them or when to use them.
I will see if this could be a knowledge base..
Posted: 2021-06-29 11:26 PM
This reply was originally posted by E. on APC forums on 9/20/2013
I think I see from the circuit diagram how they would work to bypass a circuit, but I won't say it here in case I'm wrong.
I think it would be helpful to have something authoritative. After all, these are critical circuits I'm moving onto an electronic device with, no offense, a two year warranty, and if I understand you, if it fails my critical circuits fail.
Also, kudos to the engineers for providing a simple way to restore functionality if the panel fails.
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.