Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79390members
344128posts

UPS turns off

Solved
jokerl90_apc
Crewman
Crewman
0 Likes
1
68

UPS turns off

This was originally posted on APC forums on 10/3/2010


When I shut PC down overnight or when at work, I will find UPS off (no green light, no power to PC) when I return. I have heard the UPS make a single beep sound when in this off state. After I turn the UPS back on and the PC is turned on, the UPS works correctly, the Power Chute software shows no problems. I realize the battery is old (5-years), but the light to replace battery does not light, and the UPS works correctly during AC power outage.
Any ideas?

Model: Back-UPS ES 750 (BE750BB)
Serial number: AB0544144831
Firmware revision: 819.z2.D
USB firmware revision: z2
Last self-test date: Not Applicable
Last battery replacement: 10/29/2005
CPU: Intel Pentium
Amount of RAM: 2,048 MB
Free disk space: 32,953 MB
Software version: PowerChute Personal Edition 1.5
Operating system: Microsoft Windows XP (5.1.2600)

Message was edited by: jokerl90


Accepted Solutions
jokerl90_apc
Crewman
Crewman
0 Likes
0
68

Re: UPS turns off

This was originally posted on APC forums on 10/5/2010


Yes just doing a normal shutdown from start menu. This just started a week or so ago. Only heard the beep once.
Update; Have not had this problem the last couple of nights. Maybe a problem with AC line voltage that has been corrected?? It's very odd.

See Answer In Context

1 Reply 1
jokerl90_apc
Crewman
Crewman
0 Likes
0
69

Re: UPS turns off

This was originally posted on APC forums on 10/5/2010


Yes just doing a normal shutdown from start menu. This just started a week or so ago. Only heard the beep once.
Update; Have not had this problem the last couple of nights. Maybe a problem with AC line voltage that has been corrected?? It's very odd.