Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79278members
343949posts

Steps to migrate clients, configuration etc. from Infrastruxure Central 6.2.0.659 to StruxureWare Data Center Expert 7.2.1

Solved
bhaskar.knp_apc
Crewman
Crewman
0 Likes
1
118

Steps to migrate clients, configuration etc. from Infrastruxure Central 6.2.0.659 to StruxureWare Data Center Expert 7.2.1

This was originally posted on APC forums on 8/28/2013


Hi,

We recently moved from the Infrastruxure Central (ISX) physical appliance to StruxureWare Data Center Expert (SDCE) version 7.2.1 (VM). Is there a way I can import devices previously monitored by ISX to new SDCE?

I performed a FULL backup via ISX but when I attempt to restore a backup via SDCE, the location shows up empty. Are there any steps I need to follow to make this work?

Thank you.

Bhaskar


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
118

Re: Steps to migrate clients, configuration etc. from Infrastruxure Central 6.2.0.659 to StruxureWare Data Center Expert 7.2.1

This reply was originally posted by Anonymous on APC forums on 8/30/2013


Hi Bhaskar,

You need to be on the same version to import the backup to DCE. If you do not want to lose historical data, you need to create a backup on the physical machine but you need to be on version 7.2.1. Then you can import the backup from the physical machine to the VM. Although, once you have unlocked the VM using the activation code, you can do a discovery on the VM, and it will discover the devices on your network.

Regards,

B

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
119

Re: Steps to migrate clients, configuration etc. from Infrastruxure Central 6.2.0.659 to StruxureWare Data Center Expert 7.2.1

This reply was originally posted by Anonymous on APC forums on 8/30/2013


Hi Bhaskar,

You need to be on the same version to import the backup to DCE. If you do not want to lose historical data, you need to create a backup on the physical machine but you need to be on version 7.2.1. Then you can import the backup from the physical machine to the VM. Although, once you have unlocked the VM using the activation code, you can do a discovery on the VM, and it will discover the devices on your network.

Regards,

B