Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79287members
343962posts

Smart UPS SUA1000i Power cable?

Solved
djaby_apc
Cadet
0 Likes
3
127

Smart UPS SUA1000i Power cable?

This was originally posted on APC forums on 9/12/2011


I got my APC Smart UPS SUA1000i to connect my 3D LED TV. It's a 220-240 V UPS.

There are 2 of [these |http://www.apc.com/resource/include/techspec_index.cfm?base_sku=AP9870&tab=compare] power cords provided with the UPS.
I don't see any power cord with it. Does it come with a power cord so that I can plug the UPS into the power supply?
Also, where we connect the equipments, the pin plug sizes in the receptacle are not standard I guess? They have the flat pins. I cannot connect my USA TV which has 2 flat pins into the UPS. Neither can I connect any TV or other equipments from India which have rounded pins.

Thanks.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
127

Re: Smart UPS SUA1000i Power cable?

This reply was originally posted by Dakota on APC forums on 10/7/2011


I Think Its Dumb How They Set It Up You Can Get Adapters Here

Is This The Input Cord Here?? http://www.stayonline.com/detail.aspx?ID=16735

Ups Output Plug http://www.amazon.com/prong-Plug-Adapter-5-15R-60320-C14/dp/B004OC579E

Message was edited by: Wwallender

Message was edited by: Wwallender

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
127

Re: Smart UPS SUA1000i Power cable?

This reply was originally posted by Chris on APC forums on 9/13/2011


As you mentioned, the UPS only comes with the input cords. We do not provide output cords with the unit. This unit has standard IEC connectors on the output as well so they will work with devices with the appropriate IEC connector.

krishnapg_apc
Cadet
0 Likes
0
127

Re: Smart UPS SUA1000i Power cable?

This was originally posted on APC forums on 9/24/2011


That reply is not helpful.

Appreciate if information is provided on what kind of conversion cables should be purchased to have these UPS work fine with Indian pins (Round style ones)

BillP
Administrator Administrator
Administrator
0 Likes
0
128

Re: Smart UPS SUA1000i Power cable?

This reply was originally posted by Dakota on APC forums on 10/7/2011


I Think Its Dumb How They Set It Up You Can Get Adapters Here

Is This The Input Cord Here?? http://www.stayonline.com/detail.aspx?ID=16735

Ups Output Plug http://www.amazon.com/prong-Plug-Adapter-5-15R-60320-C14/dp/B004OC579E

Message was edited by: Wwallender

Message was edited by: Wwallender