Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79291members
343970posts

Smart UPS RT 15KVA question

Solved
HotShot_apc
Cadet
0 Likes
1
66

Smart UPS RT 15KVA question

This was originally posted on APC forums on 12/13/2011


Good Day,

I have a friend seeking advice, he is a system administrator in a company. they are going to add a 15KVA smart rt UPS to their Data Center, main power supply is 380V. the question is, is it necessary to install isolation transformer?

thanks


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
66

Re: Smart UPS RT 15KVA question

This reply was originally posted by Angela on APC forums on 12/13/2011


i am assuming it is this model? http://www.apc.com/resource/include/techspec_index.cfm?base_sku=SURT15KRMXLI&tab=models

we might want to verify but all i can say right now for sure is that it is able to take 400v 3ph, N, G, connections input (or single phase 230v). is the 380v they are inputting set up that way as well? (i assume it is buy hey i will double check).

i will see if i can find anything else out.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
67

Re: Smart UPS RT 15KVA question

This reply was originally posted by Angela on APC forums on 12/13/2011


i am assuming it is this model? http://www.apc.com/resource/include/techspec_index.cfm?base_sku=SURT15KRMXLI&tab=models

we might want to verify but all i can say right now for sure is that it is able to take 400v 3ph, N, G, connections input (or single phase 230v). is the 380v they are inputting set up that way as well? (i assume it is buy hey i will double check).

i will see if i can find anything else out.