Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2022-01-08 10:48 AM
Hi,
I have a new Smart-UPS 500 (SCL500RM1UNC) and I'm unable to get power on
Group 1: Outlet Group 1 On
Group 2: Outlet Group 2 On
They are both switched on and there is no power on the outlets. Same when I switch them off.
The battery is fully charged and the UPS is in normal state and connected to the grid.
With my other UPS'es (other models) this works perfect.
The unswitched group has power and works perfect.
Main: Unswitched Group On
Is this normal? I'm trying to find out if this one is defective or if I'm missing something.
Kind Regards
Fred.
Posted: 2022-01-12 01:04 PM
If the outlets show that they are on and no AC is available you should contact local Schneider Electric technical support for assistance.
Local support contact information will be found at this link.
https://www.apc.com/us/en/support/contact-us/index.jsp
You may need to change the region in the upper left of the contact us web page.
Posted: 2022-01-13 02:21 AM
Hi Bill,
Thanks for your reply.
I contacted support and I have done that before with another issue but I usually get no reply or sometimes months later...
APC Support really sucks here that's why I tried it here.
Kind Regards
Fred.
Posted: 2022-01-14 10:02 AM
I am sorry you are experiencing this inconvenience.
Posted: 2022-01-15 01:17 PM
Hi Bill,
See the inline reply
Have you verified the battery is connected correctly?
Yes, Visually checked it and it reports healthy.
Battery Status
State of Charge
100.0 %
Battery Voltage
15.7 VDC
Health
OK
UPS Input
Input Voltage
228.1 VAC @ 50.0 Hz
Is the unit connected to the local network, and if so, does the network card report the UPS on and output on?
Yes
UPS Output
Output Voltage
229.9 VAC @ 50.0 Hz
Load Current
0.0 Amps
Output VA
0.0 %
Output Watts
0.0 %
Output Energy Usage
17.38 kWh
Outlet Group Status
Group State
Main: Unswitched Group On
Group 1: Outlet Group 1 On
Group 2: Outlet Group 2 On
Only the unswitched group has power.
Is the UPS connected to the SmartConnect portal, has it been registered, and what is the product ID?
No it's not connected to the smartportal and not registered.
About UPS
Model
Smart-UPS 500
SKU
SCL500RM1UNC
Serial Number
5S2112T52850
Firmware Revision
UPS 02.5 (ID1029)
Manufacture Date
03/28/2021
Apparent Power Rating
500 VA
Real Power Rating
400 W
Battery SKU
APCRBC167-LI
Posted: 2022-01-18 12:46 AM
I called support again today and was promised they are going to take up the case.
Let's see if I hear something back from them in the next days.
Posted: 2022-01-18 12:41 PM
Hi,
The SCL5000RM1UNC is designed for
Posted: 2022-01-19 01:41 AM
Hi Bill,
It's a SCL500RMi1UNC. But there is something wrong with it.
I send them logs and screenshots.
They agreed to swap it.
Just waiting to hear when they want to do the swap now.
Posted: 2022-01-19 01:52 AM
I see what's going on now.
The box and the back of the device says it's a SCL500RMi1UNC but the SKU says SCL500RM1UNC
I guess this device was made on a Monday morning 😛
Also the Quality Assurance test is not signed. but passed. And it reports SCL500RMi1UNC
Posted: 2022-02-01 09:31 AM
I received a new UPS today same model but this one is working perfectly.
Thanks everyone 🙂
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.