Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79278members
343949posts

Self Test a UPS

Solved
maway_at_yahoo.com_apc
Crewman
Crewman
0 Likes
2
113

Self Test a UPS

This was originally posted on APC forums on 9/15/2011


Hey,

Wondering how I can self test my Back-UPS RS 800 without it being hooked to a computer. It has a couple of switches on it and thats it. Don't know if there is a way to self test it like this or do I need to hook to a computer to test?

Only other way I can think of is to just unplug it from outlet and see how long it last.

Any help is appreciated.

Thanks

Tags (1)

Accepted Solutions
maway_at_yahoo.com_apc
Crewman
Crewman
0 Likes
0
113

Re: Self Test a UPS

This was originally posted on APC forums on 9/15/2011


Thanks for the info!

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
113

Re: Self Test a UPS

This reply was originally posted by Angela on APC forums on 9/15/2011


you should be able to hold down the power button for a second or two in order to do this manually. if you press and hold the button, the UPS will turn off so just be careful. the UPS is programmed to do a self test automatically every two weeks by the way.

here is the BR800 user's guide i referenced: http://www.apcmedia.com/salestools/ASTE-6Z7V3J_R0_EN.pdf

maway_at_yahoo.com_apc
Crewman
Crewman
0 Likes
0
114

Re: Self Test a UPS

This was originally posted on APC forums on 9/15/2011


Thanks for the info!