Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80823members
346893posts

SRT2200 / SRT3000 Configuring Outlet Group to switch on after mains input present

Solved
Rooster_apc
Ensign
Ensign
0 Likes
1
141

SRT2200 / SRT3000 Configuring Outlet Group to switch on after mains input present

This was originally posted on APC forums on 4/7/2017


Hi. we have a number of SRT2200 and SRT3000 UPS' all fitted with NMC2 Management Cards. I need the Output Groups to automatically enable once mains input is applied. I've been through all the options in the Management Card (V6.4) but cannot get them to do this. Am I missing something? Thanks.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
141

Re: SRT2200 / SRT3000 Configuring Outlet Group to switch on after mains input present

This reply was originally posted by Vinay on APC forums on 4/7/2017


Hi Richard,

Outlet groups are turned on automatically until and unless they are configured to be in off state. Make sure the outlet groups are turned on and the "stay off after power returns" options is unchecked in the outlet group configuration section.

See Answer In Context

Attachments
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
142

Re: SRT2200 / SRT3000 Configuring Outlet Group to switch on after mains input present

This reply was originally posted by Vinay on APC forums on 4/7/2017


Hi Richard,

Outlet groups are turned on automatically until and unless they are configured to be in off state. Make sure the outlet groups are turned on and the "stay off after power returns" options is unchecked in the outlet group configuration section.

Attachments