Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79290members
343968posts

Replace batteries or entire UPS in 2 x BP500CLRs?

Solved
goldcoastjon_apc
Cadet
0 Likes
1
56

Replace batteries or entire UPS in 2 x BP500CLRs?

This was originally posted on APC forums on 11/5/2012


We have owned two BP500 CLRs for about 10 years and are now replacing both of the Apple Mac g4 computers they protected.

Both batteries have been replaced once and need replacing again.

Should we replace just the batteries (about $60-$75 for 2) or buy new backup units?

I'm not sure what wattage/VA range to buy in a replacement UPS but we each now have Mac Book Pros
connected to am Ethernet switch, DSL router, and HP all-in-one printer/fax/copier/scanner (HP 7310).

Which two UPSes should we get for good auto-shutdown protection?

Do we need Pros to get the auto-shutdown?

Thanks,

Jon


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
56

Re: Replace batteries or entire UPS in 2 x BP500CLRs?

This reply was originally posted by Angela on APC forums on 11/6/2012


most UPSs provide auto-shutdown besides BE350G i think.

if BP500CLR is working fine with your new set up, just stay in the same VA range unless you want more runtime. you could trade in your current units towards a new UPS (and get a discount) and then get a new UPS with new battery and 3 year warranty on both UPS and battery.

a unit to check out might be BE550G. if you want a LCD screen on the UPS and a few other features like Automatic Voltage Regulation, check out the current Pro models: http://www.apc.com/products/family/index.cfm?id=27

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
57

Re: Replace batteries or entire UPS in 2 x BP500CLRs?

This reply was originally posted by Angela on APC forums on 11/6/2012


most UPSs provide auto-shutdown besides BE350G i think.

if BP500CLR is working fine with your new set up, just stay in the same VA range unless you want more runtime. you could trade in your current units towards a new UPS (and get a discount) and then get a new UPS with new battery and 3 year warranty on both UPS and battery.

a unit to check out might be BE550G. if you want a LCD screen on the UPS and a few other features like Automatic Voltage Regulation, check out the current Pro models: http://www.apc.com/products/family/index.cfm?id=27