Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80771members
346785posts

Repair or discard? BE550G ...

divide_by_zero
Cadet
0 Likes
1
99

Repair or discard? BE550G ...

While testing a BE550G, I connected a 40-watt string of novelty lights and they have a slight, rapid flicker with no apparent pattern. I put that battery in another 550 and the test lights are stable.

 

The unit was made in 2012. Is there a known practical fix or given its age should it be thrown away?

Tags (1)
1 Reply 1
ant_apc
Lieutenant
Lieutenant

Re: Repair or discard? BE550G ...

I'd recycle it if it is that old and not working correctly with another battery.

Tags (1)