Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-07-29 10:19 PM
This question was originally posted by juyoung on APC forums on 3/30/2011
These are possible errors which I got from root account. And it doesn't even display GUI for installation wizard.
But when I install not in root, it displays GUI but complains of not being root.
I don't think it is disk, access, OS or anti-virus issue because it proceed far well when I am not in root mode.
Also there are 100 GB free space in Ultra 10 and OS is Solaris 5.8 and JVM version is 1.6.0_19.
Is there any solution for this ?
Posted: 2021-07-29 10:19 PM
This was originally posted on APC forums on 8/2/2012
Thank you for the response.
I downloaded the following:
"PowerChute Business Edition 5 Node v9.0.1" for Solaris SPARC version. The file name is "pbe_agent_solaris_jvm.bin".
I copied it over to unix server into a directory /opt/PowerChute and type "./pbe_agent_solaris_jvm.bin". I think I also changed the permission (chmod +x pbe_agent_solaris_jvm.bin).
I try to run "./pbe_agent_solaris_jvm.bin" as root and as a normal user and none is working.
Can you tell me what I am still doing wrong?
Thanks
Paul
Posted: 2021-07-29 10:19 PM
This was originally posted on APC forums on 8/1/2012
I am having exactly the same issue. Any resolution on this please ?
Solaris 10 on Sparc T5440 server
Thanks in advance
Paul
Posted: 2021-07-29 10:19 PM
This reply was originally posted by Chris on APC forums on 8/1/2012
First of all, we want to make sure the correct version was downloaded and we are following the correct installation instructions. When you download the software, it asks you which OS you are using, X86 or non X86. Assuming you downloaded the correct one, which command are you running to run the installer?
Posted: 2021-07-29 10:19 PM
This was originally posted on APC forums on 8/2/2012
Thank you for the response.
I downloaded the following:
"PowerChute Business Edition 5 Node v9.0.1" for Solaris SPARC version. The file name is "pbe_agent_solaris_jvm.bin".
I copied it over to unix server into a directory /opt/PowerChute and type "./pbe_agent_solaris_jvm.bin". I think I also changed the permission (chmod +x pbe_agent_solaris_jvm.bin).
I try to run "./pbe_agent_solaris_jvm.bin" as root and as a normal user and none is working.
Can you tell me what I am still doing wrong?
Thanks
Paul
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.