Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79533members
344359posts

PRTK Code Problem

Solved
Castle_Romeo_apc
Crewman
Crewman
0 Likes
1
338

PRTK Code Problem

This was originally posted on APC forums on 6/11/2011


Yes,
I have a BackUPS Pro 1400 APC UPS hooked up to my computer. I also have an ULTRA BP1000A UPS hooked up to the same machine (for peripherals). I plan on using the UPSMon software as it's the only software compaible with both UPS's. Each of the two have a serial port for monitoring via desktop computer and I have the right APC cable for the BackUPS Pro. I need the PRTK code in order for the APC UPS to communicate with the UPSMon software.

I contacted the APC staff via support ticked and I was told that the codes are proprietary even though I OWN this UPS unit. I purchased it online.

The PRTK code is NOT printed on the back, BTW.

PLEASE HELP!!!


Accepted Solutions
juangele_apc
Lt. Commander
Lt. Commander
0 Likes
0
338

Re: PRTK Code Problem

This was originally posted on APC forums on 6/12/2011


Hi Castle,

If you have the right serial cable (940-0020x) of the Back UPS Pro unit, I would suggest you to use the [PowerChute Business Edition|http://www.apc.com/tools/download/index.cfm] and install the Agent for better monitoring of the UPS, instead of requesting for the UPSLink Language.

See Answer In Context

1 Reply 1
juangele_apc
Lt. Commander
Lt. Commander
0 Likes
0
339

Re: PRTK Code Problem

This was originally posted on APC forums on 6/12/2011


Hi Castle,

If you have the right serial cable (940-0020x) of the Back UPS Pro unit, I would suggest you to use the [PowerChute Business Edition|http://www.apc.com/tools/download/index.cfm] and install the Agent for better monitoring of the UPS, instead of requesting for the UPSLink Language.