Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79353members
344047posts

PNOTEPROC6 IEC standards compliance

Solved
steves741_apc
Crewman
Crewman
0 Likes
4
126

PNOTEPROC6 IEC standards compliance

This was originally posted on APC forums on 1/13/2021


Hi all, searching for a low cost surge protector that could protect both AC supply side and line (phone/DSL) side of a piece of network equipment I came across this PNOTEPROC6 surge protector, which looks promising on the surface. However, a particular requirement we have is that any device we employ should ideally conform with the new standard for MOVs used in surge protection circuits (IEC62368-1), rather than the earlier standard (IEC60950-1). For this class of surge protector the principal additional requirement seems to be the addition of thermal protection fuses in parallel with the MOVs, or the use of TP-MOVs in lieu of MOVs, to prevent the risk of fire under certain conditions. I note the words in the product brochure "Reliable thermal fusing helps ensure safe operation under all conditions", which suggests that the design may comply already (and that maybe the brochure hasn't been updated accordingly?), or perhaps would pass certification in its current form if needed.

Can anyone help me address this topic? Maybe I can break it down to a few questions in this way:

Is the unit in question already certified to conform to the IEC62368-1 standard?

If not, are there any plans for adding this certification?

If not, does the design of the unit suggest that it would be likely to comply? If so, evidence to that effect in the form of a circuit schematic would be brilliant. 

Fantastic if anyone can help!


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
126

Re: PNOTEPROC6 IEC standards compliance

This reply was originally posted by Matt on APC forums on 1/25/2021


Hi Ryan

I've just answered this question for another customer. Our compliance team are in contact with VDE to look at updating the certification for these products.  They are quite an old design and so may need a change in design or components to meet the new standard.

Regards

 

Matt

See Answer In Context

4 Replies 4
BillP
Administrator Administrator
Administrator
0 Likes
0
126

Re: PNOTEPROC6 IEC standards compliance

This reply was originally posted by Gavan on APC forums on 1/14/2021


For a question like this I'd recommend you contact your local support team, they'll be able to escalate it to the appropriate person.

-Gavan 

steves741_apc
Crewman
Crewman
0 Likes
0
126

Re: PNOTEPROC6 IEC standards compliance

This was originally posted on APC forums on 1/14/2021


Thanks Gavan but I tried them first. This was their suggestion.

Steve

BillP
Administrator Administrator
Administrator
0 Likes
0
126

Re: PNOTEPROC6 IEC standards compliance

This reply was originally posted by Ryan on APC forums on 1/23/2021


IEC International Standards reflect the global consensus and distilled wisdom of many thousand technical Generally, compliance with regulations is a must.

BillP
Administrator Administrator
Administrator
0 Likes
0
127

Re: PNOTEPROC6 IEC standards compliance

This reply was originally posted by Matt on APC forums on 1/25/2021


Hi Ryan

I've just answered this question for another customer. Our compliance team are in contact with VDE to look at updating the certification for these products.  They are quite an old design and so may need a change in design or components to meet the new standard.

Regards

 

Matt