Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 07:06 AM
This was originally posted on APC forums on 9/29/2011
I used an ES700 to replace another UPC ( RS800 ) which signaled 'end of battery life'. luckely i still had an ES700 brandnew in the box, altough it had been on the shelf for 5 or 6 yrs. I got the ES700 at the same time as the RS800 but had no need for the ES700 at the time. When i unwrapped it , i connected the lead to the battery and started the unit up. it gives a continuous tome while the red light flashes. It won't stop till you switch the unit off.
What is the cause, is it the battery has been without power too long ??? can i still charge-up the unit (ignoring the long loud beep), wil it stop eventually and would i be able to use it after 16 or so hrs??
Ruud
Message was edited by: ruuddekorte
Posted: 2021-06-29 07:06 AM
This reply was originally posted by Chris on APC forums on 9/29/2011
APC Batteries should be charged to 100% within 6 months of purchase. Anything longer than that, the battery will need to be replaced.
Posted: 2021-06-29 07:06 AM
This was originally posted on APC forums on 9/29/2011
I suppose that answeres the question. will have to replace batteries for both units..
thanx
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.