Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80782members
346814posts

My computer won't turn on in battery mode (UPS brand new)

Michel777
Cadet
0 Likes
1
94

My computer won't turn on in battery mode (UPS brand new)

Hi. My computer won't turn on in battery mode with the APC BX-1500M-LM60 1500va (900w)

The consumption of my computer is approximately only 500 watts. The same UPS show this in the display but is not working in battery mode. When the electrical service fails then my UPS can't turn on my computer, because it only turns on some RGB lights. No video signal, the rest of the pc stays off. 😞

 

My UPS is totally brand new

My PC have i9 900K processor, 9 rgb fans, 1 hdd, 1 M.2 NVME, RTX 3070 and ENERMAX 1200w Platinum power supply

 

 

any solution ?

😭😢 

Tags (1)
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
40

Re: My computer won't turn on in battery mode (UPS brand new)

Hi,

 

This UPS has two outlet groups. Battery/Surge and Surge only. During a power outage the UPS provides output to the Battery/Surge outlets. The Surge only outlets are powered off.

 

  1. Is the PC plugged into one of the Battery/Surge outlets and not a surge only outlet?
  2. Does the UPS provide output to any of the Battery/Surge outlets when switched to battery?

 

 

 

Tags (1)