Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80818members
346890posts

Modem and Router Plugged In

redtail2
Cadet
0 Likes
1
116

Modem and Router Plugged In

 I have Back-UPS Model BE600M1. I just purchased this to back up my modem and router at our vacation home. I turned the union on and charged up the unit for the 24 hours they recommend. The directions say the unit will charged the battery while turned off, and plugged in a AC outlet. If that is the case, can I turn off the unit while my modem and router is plugged in, and will the battery keep up a charge to supply enough for the router and modem in case of a power outage, or do I have to have the unit always on while the modem and router in plugged in? Thanks for any help. Chris

Tags (1)
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
93

Re: Modem and Router Plugged In

@redtail2 

 

If you have the modem and router plugged into a battery/surge outlet, the outlet will switch off if you turn the UPS off. If the modem and router are plugged into a surge-only outlet, the outlet will remain energized if you turn the UPS off.

Tags (1)