Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80750members
346734posts

Lifespan of Back-UPS ES units?

Solved
jonny_apc
Cadet
0 Likes
1
105

Lifespan of Back-UPS ES units?

This was originally posted on APC forums on 12/15/2008


Excluding the battery, how long are the Back-UPS ES units meant to last?

I've had one for six years, and recently it's been failing to supply power during an outage. It seems to be switching to battery correctly, and I can hear the inverter operating, but the outlets aren't seeing any power.

Tags (1)

Accepted Solutions
Erasmus_apc
Sisko
Sisko
0 Likes
0
105

Re: Lifespan of Back-UPS ES units?

This was originally posted on APC forums on 12/15/2008


The life cycle on Back-UPS products in generally around six years, or two battery replacements. This is of course assuming good environmental conditions and only occasional power problems. Due to variables such as these it's possible for a Back-UPS unit to have a shorter, or longer lifetime.

See Answer In Context

1 Reply 1
Erasmus_apc
Sisko
Sisko
0 Likes
0
106

Re: Lifespan of Back-UPS ES units?

This was originally posted on APC forums on 12/15/2008


The life cycle on Back-UPS products in generally around six years, or two battery replacements. This is of course assuming good environmental conditions and only occasional power problems. Due to variables such as these it's possible for a Back-UPS unit to have a shorter, or longer lifetime.