Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79125members
343511posts

LED alternating green/amber with 2 short beeps every 2 seconds!!

Solved
santosh86_apc
Crewman
Crewman
0 Likes
1
63

LED alternating green/amber with 2 short beeps every 2 seconds!!

This was originally posted on APC forums on 2/12/2011


I have the BE650Y-IN model, using it for last 2.5 years. It was working fine till yesterday when the led lights started alternating amber and green giving out 2 short beeps every 2 seconds. I am able to work fine with the computer but the beep is very annoying. Can anyone tell me what might be wrong with it? I have programmed it to High sensitivity.
I spoke to APC support, they told me to use the PowerChute software to turn of the alarm. I am not really sure I should be doing that without knowing what the beep is for. In any case, I have lost the USB cable which was provided with the unit.

1. Is my battery nearing end of life?
2. Do I have to recharge it for a certain amount of time before using it again?

PS: Missed out an important point: We had a power outage just before it started behaving this way. Could that be the source?

Will greatly appreciate any help


Accepted Solutions
santosh86_apc
Crewman
Crewman
0 Likes
0
63

Re: LED alternating green/amber with 2 short beeps every 2 seconds!!

This was originally posted on APC forums on 2/16/2011


Yup...I replaced the battery and everything's fine now.
Thanks

See Answer In Context

1 Reply 1
santosh86_apc
Crewman
Crewman
0 Likes
0
64

Re: LED alternating green/amber with 2 short beeps every 2 seconds!!

This was originally posted on APC forums on 2/16/2011


Yup...I replaced the battery and everything's fine now.
Thanks