Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79161members
343633posts

Is this adapter compatible with the Back-UPS ES (BE700-UK) model?

mapc_apc
Crewman
Crewman
0 Likes
0
111

Is this adapter compatible with the Back-UPS ES (BE700-UK) model?

This was originally posted on APC forums on 2/4/2021


Hello.

My UPS model has only 4 Battery Backup output connections but my devices are five.

Can I use this adapter to connect two of my devices and then use it with the UPS?

https://www.amazon.co.uk/dp/B08533Q7JM

The final setup would be as the attached. Of course the maximum load will not exceed the UPS's maximum of 405W.

Thank you.

Attachments
Tags (3)