Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80819members
346892posts

Is there a UPS solution with 2 USB ports?

Solved
orionizer_apc
Cadet
0 Likes
3
163

Is there a UPS solution with 2 USB ports?

This was originally posted on APC forums on 5/21/2013


I have a PC and a Synology DS-213 that I'd like to use on a single UPS.  Is there anything available that will allow me to plug both my DS and my PC into via USB to signal shutdown?

Thanks!

Tags (2)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
163

Re: Is there a UPS solution with 2 USB ports?

This reply was originally posted by Angela on APC forums on 5/22/2013


Unfortunately, no. We only offer an "interface expander" for serial communication on Smart UPS and larger UPSs. No USB expanders.

I know some SANs and NAS devices could monitor the UPS via SNMP rather than USB. Thus, if you got an APC Network Management Card in a Smart UPS for example, you could use that for managing and monitoring your UPS and for SNMP support as well as for your PC with power PowerChute Network Shutdown, or in certain instances, maybe via USB or serial at the same time as well depending on UPS model.

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
163

Re: Is there a UPS solution with 2 USB ports?

This reply was originally posted by Angela on APC forums on 5/23/2013


Thanks. I have also mentioned this feature for our next generation interface expander (but that will only work with Smart UPS and larger). I am not sure if Back UPS will ever support multiple USB connections but I can ask.

orionizer_apc
Cadet
0 Likes
0
163

Is there a UPS solution with 2 USB ports?

This was originally posted on APC forums on 5/21/2013


I have a PC and a Synology DS-213 that I'd like to use on a single UPS.  Is there anything available that will allow me to plug both my DS and my PC into via USB to signal shutdown?

Thanks!

BillP
Administrator Administrator
Administrator
0 Likes
0
164

Re: Is there a UPS solution with 2 USB ports?

This reply was originally posted by Angela on APC forums on 5/22/2013


Unfortunately, no. We only offer an "interface expander" for serial communication on Smart UPS and larger UPSs. No USB expanders.

I know some SANs and NAS devices could monitor the UPS via SNMP rather than USB. Thus, if you got an APC Network Management Card in a Smart UPS for example, you could use that for managing and monitoring your UPS and for SNMP support as well as for your PC with power PowerChute Network Shutdown, or in certain instances, maybe via USB or serial at the same time as well depending on UPS model.