Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79160members
343629posts

Is it safe to run my sony xbr960 34 HDTV CRT on my Simulated sine wave UPS?

Solved
Cube_apc
Crewman
Crewman
0 Likes
3
97

Is it safe to run my sony xbr960 34 HDTV CRT on my Simulated sine wave UPS?

This was originally posted on APC forums on 2/28/2013


Is it safe to run my sony xbr960 34 HDTV CRTon my Simulated sine wave  UPS or will it cause damage long term if it is not a real pure sine wave UPS?
I will only have the TV plugged in, nothing else.
I have an extra APC hanging around but it is a simulated sine wave or Modified Square Wave Form what ever they call it now

Tags (1)

Accepted Solutions
Cube_apc
Crewman
Crewman
0 Likes
0
97

Re: Is it safe to run my sony xbr960 34 HDTV CRT on my Simulated sine wave UPS?

This was originally posted on APC forums on 2/28/2013


UPS XS1500LCD is the APC ups. it used to come up in search on APC site but dont anymore and they make finding the page as hard as possible it point me the new models not the 2007 models when i search for it.

APC Back-UPS XS 1500 LCD



APC Back-UPS XS 1500 LCD - Reviews & Prices @ Yahoo! Shopping


I used a sim sinewave UPS on a cheeper Sony TV so when I play games I can save and turn them off  or when I come back from like lunch it will still be going  and i wont lose my spot and it seem to have died a quicker death   My sony xbr960 I do not even want to risk it. I only need it to power the TV for like 9 minutes at max to ride  out quick power outages or finish what parts of the games I am on.

I guess it is safe for game consoles because they are  just Tiny PCs and this is a PC UPS the tube is what I am worried about hurting the most.

it is what is called a step wave.... I also have a simulated sinewave one  but can not find the model number it had stickers over it and i cant get all of it off to read it numbers.  My new ones are real sine wave output but i use them on PCs.

unless it is safer to use it just on surge only..
.

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
97

Re: Is it safe to run my sony xbr960 34 HDTV CRT on my Simulated sine wave UPS?

This reply was originally posted by Bernard on APC forums on 2/28/2013


Good day Cube,

Can you tell us what the part number is of the APC UPS that's hanging around? You can get the part number from the white sticker with bar codes usually at the bottom or at the back of the UPS. Have you tried to get in touch with Sony to find out if the power requirements of your hdtv?

BillP
Administrator Administrator
Administrator
0 Likes
0
97

Re: Is it safe to run my sony xbr960 34 HDTV CRT on my Simulated sine wave UPS?

This reply was originally posted by Joe on APC forums on 2/28/2013


I have a Sony XBR9 40" LCD flat screen on a small, 750VA, APC UPS with a stepped approximation of a sine wave output.  The TV operates "almost" OK as there is a slight "hum" in the audio output probably due to the distortion on the UPS output.  The picture, however, is fine.  My situation and experience causes me to believe it will NOT cause a problem long term as the commercial power in my area is pretty stable so the TV is not on the UPS that often.

Cube_apc
Crewman
Crewman
0 Likes
0
98

Re: Is it safe to run my sony xbr960 34 HDTV CRT on my Simulated sine wave UPS?

This was originally posted on APC forums on 2/28/2013


UPS XS1500LCD is the APC ups. it used to come up in search on APC site but dont anymore and they make finding the page as hard as possible it point me the new models not the 2007 models when i search for it.

APC Back-UPS XS 1500 LCD



APC Back-UPS XS 1500 LCD - Reviews & Prices @ Yahoo! Shopping


I used a sim sinewave UPS on a cheeper Sony TV so when I play games I can save and turn them off  or when I come back from like lunch it will still be going  and i wont lose my spot and it seem to have died a quicker death   My sony xbr960 I do not even want to risk it. I only need it to power the TV for like 9 minutes at max to ride  out quick power outages or finish what parts of the games I am on.

I guess it is safe for game consoles because they are  just Tiny PCs and this is a PC UPS the tube is what I am worried about hurting the most.

it is what is called a step wave.... I also have a simulated sinewave one  but can not find the model number it had stickers over it and i cant get all of it off to read it numbers.  My new ones are real sine wave output but i use them on PCs.

unless it is safer to use it just on surge only..
.