Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80694members
346646posts

How do I upgrade firmware on SC1500?

Solved
Hestpeisen_apc
Crewman
Crewman
0 Likes
2
110

How do I upgrade firmware on SC1500?

This was originally posted on APC forums on 2/3/2020


I have an old SC1500 running a server at my cabin on an island here in Norway, where the power is not all that reliable. I wanted to upgrade the firmware and downloaded the Firmware Upgrade Wizard, version 4.1.1. But it can't find the UPS. I have exited PowerChute Business Edition (which was of course blocking the port), but that didn't help. I have also tried to use a Windows 7 backup OS that I have on another partition on the server, so there has been no PowerChute installed there. That didn't help either. Do I need another version of that program? I do not have the original serial cable, but it is patched to be like it. And I doubt that it is the cable since PowerChute works without a hitch. Can somebody please direct me to a solution?

Tags (1)

Accepted Solutions
Hestpeisen_apc
Crewman
Crewman
0 Likes
0
110

Re: How do I upgrade firmware on SC1500?

This was originally posted on APC forums on 2/3/2020


That explains it, thanks! Rather weird that there is a firmware downloadable from the product page then, isn't it? winkIt's no biggie, I was actually only trying to find firmware where I could set the timeout for the PowerChute connection to more than 10 minutes, it drives me nuts when breaking in new batteries, I want to follow the percentage.

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
110

Re: How do I upgrade firmware on SC1500?

This reply was originally posted by Bill on APC forums on 2/3/2020


Hi,

That model UPS does not have upgradeable firmware. If you are looking for a Smart-UPS with upgradeable firmware the models are SMT, SMX, SMC, and SRT. 

Hestpeisen_apc
Crewman
Crewman
0 Likes
0
111

Re: How do I upgrade firmware on SC1500?

This was originally posted on APC forums on 2/3/2020


That explains it, thanks! Rather weird that there is a firmware downloadable from the product page then, isn't it? winkIt's no biggie, I was actually only trying to find firmware where I could set the timeout for the PowerChute connection to more than 10 minutes, it drives me nuts when breaking in new batteries, I want to follow the percentage.