Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 08:05 PM
This was originally posted on APC forums on 8/6/2009
Only the surge protection end of my battery back up is working. The end that says battery backup + surge protection does not function. Do I need to replace the battery or the whole unit? Can anyone help? Thanks!
These are the numbers on the botton:
BE325R
4BO532P51966
Posted: 2021-06-29 08:06 PM
This was originally posted on APC forums on 8/6/2009
The clear button is used to Power on/off the unit. The UPS should respond when you press the Power on button.
The Circuit breaker is located near the UPS input power cord.
This unit will emit the Replacement Battery warning alarm and visual indication if the battery needs replacement. However, it is not powering on which leads to believe that there is an internal fault in the unit not the battery.
Posted: 2021-06-29 08:05 PM
This was originally posted on APC forums on 8/6/2009
Sandee,
Is the UPS powering on? Do you see a green light on the unit? Could you please try resetting the UPS circuit breaker and check if that works out?
Posted: 2021-06-29 08:05 PM
This was originally posted on APC forums on 8/6/2009
I'm not sure what to reset...I don't see a green light either. There is a clear button on top, but it doesn't do anything when pressed.
Posted: 2021-06-29 08:06 PM
This was originally posted on APC forums on 8/6/2009
The clear button is used to Power on/off the unit. The UPS should respond when you press the Power on button.
The Circuit breaker is located near the UPS input power cord.
This unit will emit the Replacement Battery warning alarm and visual indication if the battery needs replacement. However, it is not powering on which leads to believe that there is an internal fault in the unit not the battery.
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.