Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79201members
343759posts

Half of my battery back up works???

Solved
Sandee_apc
Cadet
0 Likes
3
109

Half of my battery back up works???

This was originally posted on APC forums on 8/6/2009


Only the surge protection end of my battery back up is working. The end that says battery backup + surge protection does not function. Do I need to replace the battery or the whole unit? Can anyone help? Thanks!

These are the numbers on the botton:
BE325R
4BO532P51966


Accepted Solutions
Techie_apc
Admiral
Admiral
0 Likes
0
109

Re: Half of my battery back up works???

This was originally posted on APC forums on 8/6/2009


The clear button is used to Power on/off the unit. The UPS should respond when you press the Power on button.
The Circuit breaker is located near the UPS input power cord.

This unit will emit the Replacement Battery warning alarm and visual indication if the battery needs replacement. However, it is not powering on which leads to believe that there is an internal fault in the unit not the battery.

See Answer In Context

3 Replies 3
Techie_apc
Admiral
Admiral
0 Likes
0
109

Re: Half of my battery back up works???

This was originally posted on APC forums on 8/6/2009


Sandee,

Is the UPS powering on? Do you see a green light on the unit? Could you please try resetting the UPS circuit breaker and check if that works out?

Sandee_apc
Cadet
0 Likes
0
109

Re: Half of my battery back up works???

This was originally posted on APC forums on 8/6/2009


I'm not sure what to reset...I don't see a green light either. There is a clear button on top, but it doesn't do anything when pressed.

Techie_apc
Admiral
Admiral
0 Likes
0
110

Re: Half of my battery back up works???

This was originally posted on APC forums on 8/6/2009


The clear button is used to Power on/off the unit. The UPS should respond when you press the Power on button.
The Circuit breaker is located near the UPS input power cord.

This unit will emit the Replacement Battery warning alarm and visual indication if the battery needs replacement. However, it is not powering on which leads to believe that there is an internal fault in the unit not the battery.