Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 12:02 AM
This was originally posted on APC forums on 2/4/2009
Dear Alls
I new member. I want to ask all of you about my problem as follow :
Now I using one UPS APC 5K for server system, and used one invidual Generator (5,5KVA) for that UPS. When main electric source cut off, Generator runing normally (Voltage, capacity,frequency..) but UPS did not received source of Generator (It was good condition at some week after installation generator). Please let me know why, how to solve... ?
Thanks so much
Posted: 2021-06-29 12:02 AM
This reply was originally posted by Angela on APC forums on 2/4/2009
which UPS is this? do you have a specific model?
depending on the model and the topology, there will be a sensitivity button/LED on the back you can try adjusting.
also, how did you verify the incoming voltage/frequency was within range of what the UPS can accept?
i posted a couple articles below that may help as well..
[General generator information that I kind of summarized|http://nam-en.apc.com/cgi-bin/nam_en.cfg/php/enduser/std_adp.php?p_faqid=7354]
[Generator sizing|http://nam-en.apc.com/cgi-bin/nam_en.cfg/php/enduser/std_adp.php?p_faqid=7300]
Posted: 2021-06-29 12:02 AM
This reply was originally posted by Angela on APC forums on 2/9/2009
okay, this model doesnt have an LED button on it. you should be able to adjust the sensitivity via the network management card or in the menu on the front of the UPS. are you able to get to the front of the UPS menu and look for the sensitivity option in the menus? You can try adjusting it to low if its not there already.
if it is already on low, you wont be able to do anything else and may have to look into tweaking the generator.
Posted: 2021-06-29 12:02 AM
This was originally posted on APC forums on 2/10/2009
Now i have a solotion as :
When Electric source shut down, I run Generator and change UPS to bypass mode, it's ok or not !?
Posted: 2021-06-29 12:02 AM
This reply was originally posted by Angela on APC forums on 2/10/2009
yeah you can do that but it is not recommended, especially if there is a problem with generator power that could cause harm to your load (which is why the UPS goes to battery on generator most likely).
Posted: 2021-06-29 12:02 AM
This was originally posted on APC forums on 2/5/2009
Thanks for your supported !
Posted: 2021-06-29 12:02 AM
This was originally posted on APC forums on 2/9/2009
Dear Sir
My UPS model is APC MATRIC 5000VA.
So you know how to adjusted ? LED button what is mean ?
Thanks
Posted: 2021-06-29 12:02 AM
This reply was originally posted by Angela on APC forums on 2/4/2009
which UPS is this? do you have a specific model?
depending on the model and the topology, there will be a sensitivity button/LED on the back you can try adjusting.
also, how did you verify the incoming voltage/frequency was within range of what the UPS can accept?
i posted a couple articles below that may help as well..
[General generator information that I kind of summarized|http://nam-en.apc.com/cgi-bin/nam_en.cfg/php/enduser/std_adp.php?p_faqid=7354]
[Generator sizing|http://nam-en.apc.com/cgi-bin/nam_en.cfg/php/enduser/std_adp.php?p_faqid=7300]
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.