Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79138members
343551posts

Force AVR Threshold

Solved
harrypelles_apc
Crewman
Crewman
0 Likes
5
160

Force AVR Threshold

This was originally posted on APC forums on 6/21/2007


Hi Everyone,

I just bought a BX1300LCD (Smart UPS).

In the PowerChute software, the configurable range of voltage thresholds for AVR is somewhere like 88 (min.) and 139 (max.). The 88 minimum thresholds seems to me to be essentially useless.

Does anyone know of a way to force the AVR threshold minimum up to somewhere around 115 or so? Ideally I'd like to keep the voltage range at 120 +/- 5.

Any help greatly appreciated.

Thanks!


Accepted Solutions
harrypelles_apc
Crewman
Crewman
0 Likes
0
161

Re: Force AVR Threshold

This was originally posted on APC forums on 6/22/2007


Anyone else out there have ideas that could help?

Any way I might be able to fool the PowerChute (linux or windows version) software into letting me set a higher (low) threshold?

Thanks again.

See Answer In Context

5 Replies 5
harrypelles_apc
Crewman
Crewman
0 Likes
0
161

Re: Force AVR Threshold

This was originally posted on APC forums on 6/21/2007


I'd also like to mention that I installed the PowerChute Business for Linux and tried the init and config scripts, editing the config file, etc. to force a threshold value. All were with no luck. Thanks!

Sgt._Slaughter_apc
Lt. Commander
Lt. Commander
0 Likes
0
161

Re: Force AVR Threshold

This was originally posted on APC forums on 6/21/2007


What version of Business Edition are you using? Which cable? Is it possible to hook the unit up to a Windows Machine and use Personal Edition to adjust the Low Transfer Voltage setting? Is that option available in the Agent interface for this UPS under Configuration?

Thanks.

harrypelles_apc
Crewman
Crewman
0 Likes
0
161

Re: Force AVR Threshold

This was originally posted on APC forums on 6/21/2007


The business version is v7.0.5 Agent for Linux.

I can connect a windows machine to the UPS and change the settings in the PowerChute (v2.0) software, but the highest, low threshold is 88 Volts. I'd like to force the low threshold to somewhere around 110 to 115 or so.

I also tried setting the LOTRANSFER value to something higher in the linux version config file and reloading, but no luck.

Message was edited by: harrypelles

harrypelles_apc
Crewman
Crewman
0 Likes
0
161

Force AVR Threshold

This was originally posted on APC forums on 6/21/2007


Hi Everyone,

I just bought a BX1300LCD (Smart UPS).

In the PowerChute software, the configurable range of voltage thresholds for AVR is somewhere like 88 (min.) and 139 (max.). The 88 minimum thresholds seems to me to be essentially useless.

Does anyone know of a way to force the AVR threshold minimum up to somewhere around 115 or so? Ideally I'd like to keep the voltage range at 120 +/- 5.

Any help greatly appreciated.

Thanks!

harrypelles_apc
Crewman
Crewman
0 Likes
0
162

Re: Force AVR Threshold

This was originally posted on APC forums on 6/22/2007


Anyone else out there have ideas that could help?

Any way I might be able to fool the PowerChute (linux or windows version) software into letting me set a higher (low) threshold?

Thanks again.