Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80634members
346600posts

Flat APC UPS with real-time on screen status?

ant_apc
Lieutenant
Lieutenant
0 Likes
0
87

Flat APC UPS with real-time on screen status?

This was originally posted on APC forums on 5/2/2021


Does one exists? I have a decade old APC Back-UPS ES-750(BE750G) with its dead battery #2, but I don't like its lack of detailed status on its physical device like my vertical APC Back-UPS XS 1500 (model: BX1500G). Also, I hated how replacing its batteries are difficult due to short red and black cables. I like the tall tower UPS' batteries that can be removed and installed without any cables. However, I don't want the tower one though since the area I want to put it has little height room (9"). I would also like to have it hold up to 600 watts under heavy loads.

Thank you for reading and hopefully answering. 🙂