Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80704members
346658posts

Finding correct replacement battery model (RBC#) for Backup-UPS RS BR1500I (SB-12)

Solved
joan_yeo_apc
Crewman
Crewman
0 Likes
2
176

Finding correct replacement battery model (RBC#) for Backup-UPS RS BR1500I (SB-12)

This was originally posted on APC forums on 5/20/2014


I have a APS Back-UPS RS model with a faulty battery, and I have been trying to find the correct battery model to replace it. This UPS unit was bought in September 2009.

When I called Schneider Electric (Singapore) to find out which battery model I should purchase, they requested a RBC number (RBC#). I have been looking for the RBC number on my APC unit as well as on the faulty battery pack, but I cannot find it.

I hope that experienced users here can give me an idea of what the correct replacement model number is.

The purchase information of the UPS unit is as follows:

APC Back-UPS RS

1500VA / 865W

Input 230V / Output 230V

Interface Port USB

Extended runtime model

Rack Height 2 U

Product: BR1500I (SB-12)

Serial Number : BB0911009747

UPC: 731304193173

I have included pictures of various numbers and stickers on the UPS unit and battery.

Any and all help will be greatly appreciated.

2364_IMG-20140520-WA0009.jpg

2365_IMG-20140520-WA0012.jpg

2366_IMG-20140520-WA0013.jpg

2368_20140520_140507.jpg

2369_20140520_140522.jpg

2371_20140520_140629.jpg

2370_20140520_140608.jpg


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
176

Re: Finding correct replacement battery model (RBC#) for Backup-UPS RS BR1500I (SB-12)

This reply was originally posted by Bill on APC forums on 5/21/2014


Hi,

Here is a link to the technical specifications for your BR1500i http://www.apc.com/products/resource/include/techspec_index.cfm?base_sku=BR1500I

The tech specs list RBC33 as the proper replacement battery Buy APC Replacement Battery Cartridge #33 - Technical Specifications and Information | APC

See Answer In Context

2 Replies 2
joan_yeo_apc
Crewman
Crewman
0 Likes
0
177

Re: Finding correct replacement battery model (RBC#) for Backup-UPS RS BR1500I (SB-12)

This was originally posted on APC forums on 5/21/2014


Searching "OM-1332" on this forum shows that the battery pack I need could be either an RBC-32 or RBC-33.

http://forums.apc.com/message/31119#31119

http://forums.apc.com/message/32910#32910

What is the difference between the RBC-32 or RBC-33 and which one should I get?


BillP
Administrator Administrator
Administrator
0 Likes
0
177

Re: Finding correct replacement battery model (RBC#) for Backup-UPS RS BR1500I (SB-12)

This reply was originally posted by Bill on APC forums on 5/21/2014


Hi,

Here is a link to the technical specifications for your BR1500i http://www.apc.com/products/resource/include/techspec_index.cfm?base_sku=BR1500I

The tech specs list RBC33 as the proper replacement battery Buy APC Replacement Battery Cartridge #33 - Technical Specifications and Information | APC