Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 12:03 AM
This was originally posted on APC forums on 5/20/2014
I have a APS Back-UPS RS model with a faulty battery, and I have been trying to find the correct battery model to replace it. This UPS unit was bought in September 2009.
When I called Schneider Electric (Singapore) to find out which battery model I should purchase, they requested a RBC number (RBC#). I have been looking for the RBC number on my APC unit as well as on the faulty battery pack, but I cannot find it.
I hope that experienced users here can give me an idea of what the correct replacement model number is.
The purchase information of the UPS unit is as follows:
APC Back-UPS RS
1500VA / 865W
Input 230V / Output 230V
Interface Port USB
Extended runtime model
Rack Height 2 U
Product: BR1500I (SB-12)
Serial Number : BB0911009747
UPC: 731304193173
I have included pictures of various numbers and stickers on the UPS unit and battery.
Any and all help will be greatly appreciated.
Posted: 2021-06-30 12:03 AM
This reply was originally posted by Bill on APC forums on 5/21/2014
Hi,
Here is a link to the technical specifications for your BR1500i http://www.apc.com/products/resource/include/techspec_index.cfm?base_sku=BR1500I
The tech specs list RBC33 as the proper replacement battery Buy APC Replacement Battery Cartridge #33 - Technical Specifications and Information | APC
Posted: 2021-06-30 12:03 AM
This was originally posted on APC forums on 5/21/2014
Searching "OM-1332" on this forum shows that the battery pack I need could be either an RBC-32 or RBC-33.
http://forums.apc.com/message/31119#31119
http://forums.apc.com/message/32910#32910
What is the difference between the RBC-32 or RBC-33 and which one should I get?
Posted: 2021-06-30 12:03 AM
This reply was originally posted by Bill on APC forums on 5/21/2014
Hi,
Here is a link to the technical specifications for your BR1500i http://www.apc.com/products/resource/include/techspec_index.cfm?base_sku=BR1500I
The tech specs list RBC33 as the proper replacement battery Buy APC Replacement Battery Cartridge #33 - Technical Specifications and Information | APC
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.