Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80775members
346794posts

ES 725 Hibernates PC but immediately reboots

bradp_apc
Cadet
0 Likes
0
43

ES 725 Hibernates PC but immediately reboots

This was originally posted on APC forums on 6/15/2013


Hi

I have the ES 725 with a new battery. I also have Windows 8 with the Powerchute software 3.02

When the power is cut to the UPS, Powerchute immediately sends the PC into hibernation which is what I want. But once it finishes going into hibernation, it just reboots. For the test I did, I had unplugged the UPS. After it booted up (or perhaps it was during), I plugged the UPS back in. ONce the PC was booted, the UPS beeped a few times and the computer lost power and had a hard shutdown.

My question is why is the PC rebooting after going into hibernation? I mean it immediately reboots, there is no delay.

Thanks