Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79098members
343434posts

ES 700 Constant alarm

Solved
PM_apc
Cadet
0 Likes
1
91

ES 700 Constant alarm

This was originally posted on APC forums on 1/14/2013


Hi,
I have an ES 700 and since yesterday it emits a constant alarm.

I have disconnected everything and even now when I plug it in I get get green light and after and15 seconds I get a constant warbling alarm screech with green light followed (after a minute or so) by a constant screech and no light!

It Is A BE700-uk
5B0729U04293

I replaced the battery in January 2011 with an APC battery 101003v33

Any assistance appreciated
Peter


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
91

Re: ES 700 Constant alarm

This reply was originally posted by Jonathan on APC forums on 1/17/2013


From the way that you have described the situation, it appears that you are experiencing an On-Battery Overload. Can you try to turn off the UPS and then remove the load attached to it. Once this is done, turn on the UPS once more, if the same problem occurs the UPS is damaged and should be replaced.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
92

Re: ES 700 Constant alarm

This reply was originally posted by Jonathan on APC forums on 1/17/2013


From the way that you have described the situation, it appears that you are experiencing an On-Battery Overload. Can you try to turn off the UPS and then remove the load attached to it. Once this is done, turn on the UPS once more, if the same problem occurs the UPS is damaged and should be replaced.