Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79278members
343951posts

Clicking only in sleep mode

Solved
tom_botts_apc
Cadet
0 Likes
1
112

Clicking only in sleep mode

This was originally posted on APC forums on 2/8/2013


I have a RS 1500 UPS. I am running Vista 64 bit. Lately when I put the PC in sleep mode the battery will click every few minutes. This only happens in sleep mode. If I wake the computer the UPS works fine with no clicking. Any ideas?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
112

Re: Clicking only in sleep mode

This reply was originally posted by Jonathan on APC forums on 2/8/2013


Tom,

What is the model number of the UPS that you are using? This can be found on the white barcode sticker found underneath the UPS. If you are using the latest BackUPS Pro LCD model, can you check if you have enabled the master control functionality of the UPS.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
113

Re: Clicking only in sleep mode

This reply was originally posted by Jonathan on APC forums on 2/8/2013


Tom,

What is the model number of the UPS that you are using? This can be found on the white barcode sticker found underneath the UPS. If you are using the latest BackUPS Pro LCD model, can you check if you have enabled the master control functionality of the UPS.