Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79549members
344381posts

Can I route phone line to DSL router through BackUPS RS 700?

Solved
Jelf_apc
Crewman
Crewman
0 Likes
1
80

Can I route phone line to DSL router through BackUPS RS 700?

This was originally posted on APC forums on 2/1/2011


I have a new Back-UPS RE 700. On the back are two ethernet ports (RJ45).
Is it possible to route the phone line to my DSL router/modem through those ports so my router/modem is protected from power spikes on the phone wire?

Here's what I tried.

I bought 2 plug converters so I could convert my RJ11 phone wire plugs into RJ45 plugs. I then connected the phone line from the wall to the UPS and from the UPS to my router. Internet worked just fine.

However, my telephone handset could not receive any calls. Yes, the phone line to my handset has the dsl filter thing installed.

Is there anything else I can try?

Should I have purchased a different UPS in order to protect my router/modem from phone line surges?


Accepted Solutions
Jelf_apc
Crewman
Crewman
0 Likes
0
80

Re: Can I route phone line to DSL router through BackUPS RS 700?

This was originally posted on APC forums on 2/4/2011


The model is BR700G.

This new unit replaces a LS-700 which had 2 RJ11 ports on the back.

See Answer In Context

1 Reply 1
Jelf_apc
Crewman
Crewman
0 Likes
0
81

Re: Can I route phone line to DSL router through BackUPS RS 700?

This was originally posted on APC forums on 2/4/2011


The model is BR700G.

This new unit replaces a LS-700 which had 2 RJ11 ports on the back.