Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80996members
347196posts

Cable Connection to PC for BX1500G

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
197

Cable Connection to PC for BX1500G

This question was originally posted by Allen on APC forums on 7/30/2016


Am trying to get the PowerChute software installed and am confused about connecting the BX1500G backup to my PC.  The instructions show a picture of a cable that appears to have an ethernet connection on one end and a USB on the other.  The cable that came with my unit, which is too short to be useful anyway, has the ethernet connection on both ends.

Now I am not really all that smart about this stuff but do I connect to my PC into the ehternet port or did I just get the wrong cable and need a replacement?

As an aside, finding the PowerChute download on the APC site took over an hour since the instructions in the manual are incorrect and searching the site produced too many results to be useful.  This should be easy.

Rather frustrated.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
197

Re: Cable Connection to PC for BX1500G

This reply was originally posted by Bill on APC forums on 8/1/2016


Hi,

That unit should have shipped with cable 940-0127 that is RJ50 to USB A The cable connects to the rear of the UPS in the slot labeled DataPort.

This is what the cable looks like.

If the cable has been lost you can contact local support for assistance. 

See Answer In Context

Attachments
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
198

Re: Cable Connection to PC for BX1500G

This reply was originally posted by Bill on APC forums on 8/1/2016


Hi,

That unit should have shipped with cable 940-0127 that is RJ50 to USB A The cable connects to the rear of the UPS in the slot labeled DataPort.

This is what the cable looks like.

If the cable has been lost you can contact local support for assistance. 

Attachments