Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79153members
343609posts

CORSAIR 650W with UPS Pro 1500 APC battery backup

Solved
jbaccrington_apc
Ensign
Ensign
0 Likes
1
76

CORSAIR 650W with UPS Pro 1500 APC battery backup

This was originally posted on APC forums on 11/26/2013


Hi

Just came back and turned my PC on, after about 5 to 10mins the PC Power Supply started buzzing and windows7 froze, couldn't move my mouse cursor. Had to turn the power off on the UPS using the power off switch.

I had posted before about my Pro 1500 APC battery backup causing my CORSAIR 650W to buzz during battery backup.

What options do I have?

Return the UPS?

thxs

Jonathan



Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
77

Re: CORSAIR 650W with UPS Pro 1500 APC battery backup

This reply was originally posted by Llewellyn on APC forums on 11/27/2013


Hi Johnathan,

One possible problem might be that the UPS outputs a square wave when running on battery operation. Have a look at this post:

http://www.tomshardware.com/forum/352692-28-will-corsair-work-sinwave-square-wave#.

If the UPS is a Back UPS Pro or any kind of Back UPS it produces a square wave output. You can try and get you hands on a Smart UPS which is more expensive than the Back UPS but it produces a pure sin wave output when running on battery power. A smart UPS will also be a more efficient UPS.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
78

Re: CORSAIR 650W with UPS Pro 1500 APC battery backup

This reply was originally posted by Llewellyn on APC forums on 11/27/2013


Hi Johnathan,

One possible problem might be that the UPS outputs a square wave when running on battery operation. Have a look at this post:

http://www.tomshardware.com/forum/352692-28-will-corsair-work-sinwave-square-wave#.

If the UPS is a Back UPS Pro or any kind of Back UPS it produces a square wave output. You can try and get you hands on a Smart UPS which is more expensive than the Back UPS but it produces a pure sin wave output when running on battery power. A smart UPS will also be a more efficient UPS.