Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79544members
344375posts

Backups do not work

Solved
dotcpa_apc
Cadet
0 Likes
1
61

Backups do not work

This was originally posted on APC forums on 5/5/2008


I have about 10 of these backups from APC so far. However, every time the power is interrupted, none of the computers stay on except for the laptops with batteries in them. Why don't these things keep the computers on?


Accepted Solutions
EZ_Button_apc
Commander
Commander
0 Likes
0
61

Re: Backups do not work

This was originally posted on APC forums on 5/6/2008


Check where you have the devices plugged into the UPS. Some of the outlets are "Surge Protection Only" and others provide the battery power. Obviously, make sure your computers are in the battery powered outlets.

See Answer In Context

1 Reply 1
EZ_Button_apc
Commander
Commander
0 Likes
0
62

Re: Backups do not work

This was originally posted on APC forums on 5/6/2008


Check where you have the devices plugged into the UPS. Some of the outlets are "Surge Protection Only" and others provide the battery power. Obviously, make sure your computers are in the battery powered outlets.