Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80928members
347072posts

Back UPS RS 600

Solved
ganeshanv_apc
Cadet
0 Likes
3
147

Back UPS RS 600

This was originally posted on APC forums on 11/3/2011


I purchased a back-UPS RS 600 in July 2011 from Mercy Electronics, Chennai.I've connected a desktop computer to it. I find that when power is off, the UPS shuts off within two/three minutes making the entire purchase of UPS futile...I guess that I'm missing some tricks. I would appreciate some answers to rectify this..Ganeshan, Chennai

Tags (1)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
147

Re: Back UPS RS 600

This reply was originally posted by Jonathan on APC forums on 11/3/2011


Good day Ganeshan,

I would like to know if you've installed the software that came with the unit, PowerChute Personal Edition or might be using the Native UPS software that your computer offers? This would help us analyze if the software is commanding your PC to turn off. Also, do you have any idea with the total wattage consumption of the load and the runtime that the UPS offers?

See Answer In Context

3 Replies 3
gunajoe_apc
Cadet
0 Likes
0
147

Re: Back UPS RS 600

This was originally posted on APC forums on 11/13/2011


I also have the same model. I just bought yesterday from the same shop mentioned above. My UPS didnt even power up my PC.It just provides the long constant beep. I disconnected the PC and Monitor still the same results

I Charged the UPS for about 10 hrs and tried. No use 😞 .
I tired to use the UPS battery , its works fine. When Swicth to on-line mode its working. It just give a constant beep.

Can you tell what could be the problem?

BillP
Administrator Administrator
Administrator
0 Likes
0
147

Re: Back UPS RS 600

This reply was originally posted by Jonathan on APC forums on 11/14/2011


Normally, if the UPS emits a constant beep and the unit does not provide power it is what do we call as an overload condition. Were you able to turn the UPS on without any load attached to it?

BillP
Administrator Administrator
Administrator
0 Likes
0
148

Re: Back UPS RS 600

This reply was originally posted by Jonathan on APC forums on 11/3/2011


Good day Ganeshan,

I would like to know if you've installed the software that came with the unit, PowerChute Personal Edition or might be using the Native UPS software that your computer offers? This would help us analyze if the software is commanding your PC to turn off. Also, do you have any idea with the total wattage consumption of the load and the runtime that the UPS offers?