Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79365members
344085posts

BX1500LCD Dead after power outage.

Solved
Nitro468_apc
Crewman
Crewman
0 Likes
3
118

BX1500LCD Dead after power outage.

This was originally posted on APC forums on 9/11/2012


I have an older BX1500LCD model.


The unit needed a battery, but before I got the chance to order one the power went out, and my unit is now DEAD.

I left the unit in place without the battery as protection against surges. The local utility had an issue where we lost power on one phase (the one where the UPS is on of course) It was a burnt connection in the street that affected 12 houses. Ever since that the unit will not even power up. (Better the UPS than my computer, good sacrifice).

Upon investigation, and poor cash flow, I opened up the unit. Capacitor 69 was slightly bulged so it was replaced with no success. (22 uf 400V) Physically everything looks OK on the board. I do have line in power to the board but nothing to the transformer. (Circuit breaker is good). A schematic would really be helpful here.

I really like this unit (for the gracious sacrifice it made), but I have no cash flow to buy a new unit or trade it in.

Any help would be greatly appreciated.

Thank you.


Accepted Solutions
Nitro468_apc
Crewman
Crewman
0 Likes
0
118

Re: BX1500LCD Dead after power outage.

This was originally posted on APC forums on 9/17/2012


I believe this one will start with no battery... It did in the past. Can't hurt to jump one in to see.

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
118

Re: BX1500LCD Dead after power outage.

This reply was originally posted by Chris on APC forums on 9/17/2012


We unfortunately can't give out schematics but if anyone else can help, please reply.

voidstar_apc
Janeway
Janeway
0 Likes
0
118

Re: BX1500LCD Dead after power outage.

This was originally posted on APC forums on 9/17/2012


I'm not sure about the BackUPS but some of APC's UPSes require a working battery to start up. See here.

Nitro468_apc
Crewman
Crewman
0 Likes
0
119

Re: BX1500LCD Dead after power outage.

This was originally posted on APC forums on 9/17/2012


I believe this one will start with no battery... It did in the past. Can't hurt to jump one in to see.