Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79278members
343951posts

APC Smart UPS 6000RT

Solved
yokanan_apc
Cadet
0 Likes
1
90

APC Smart UPS 6000RT

This was originally posted on APC forums on 9/29/2012


Dear all,

I Have APC Smart UPS 6000RT and I need such kind tools like :
1. Setup Email notification if there were any problems with the ups
2. Monitoring tools (Gui) of the UPS

Does any one can help me?


Thanks,



Yokanan


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
90

Re: APC Smart UPS 6000RT

This reply was originally posted by Angela on APC forums on 10/1/2012


this UPS ships with a preinstalled network management card (either AP9619 or AP9631). this is the device that will provide email notification.

our knowledge base has information on setting that up and configuring it: http://www.apc.com/site/support/index.cfm/faq/

articles to refer to:
FA156064 - will help you set up and configure the network management card with TCP/IP settings

as far as setting up email itself, there are instructions in the network management card user's guide depending on what model you have. let's assume AP9631: http://www.apcmedia.com/salestools/PMAR-8P9G2C_R2_EN.pdf

this will help with setting up an email server, adding a recipient, etc

the network management card has the following interfaces that you can access or set up for monitoring/configuration: SNMP, telnet, syslog, FTP, HTTP, HTTPS, SCP, and SSH. I think i got them all.

then for graceful shutdown of your attached devices, you'll want to look at powerchute network shutdown software and check the compatibility chart.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
91

Re: APC Smart UPS 6000RT

This reply was originally posted by Angela on APC forums on 10/1/2012


this UPS ships with a preinstalled network management card (either AP9619 or AP9631). this is the device that will provide email notification.

our knowledge base has information on setting that up and configuring it: http://www.apc.com/site/support/index.cfm/faq/

articles to refer to:
FA156064 - will help you set up and configure the network management card with TCP/IP settings

as far as setting up email itself, there are instructions in the network management card user's guide depending on what model you have. let's assume AP9631: http://www.apcmedia.com/salestools/PMAR-8P9G2C_R2_EN.pdf

this will help with setting up an email server, adding a recipient, etc

the network management card has the following interfaces that you can access or set up for monitoring/configuration: SNMP, telnet, syslog, FTP, HTTP, HTTPS, SCP, and SSH. I think i got them all.

then for graceful shutdown of your attached devices, you'll want to look at powerchute network shutdown software and check the compatibility chart.