Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79317members
344001posts

APC 900 sx no signs of life.

Solved
TTStudio_apc
Crewman
Crewman
0 Likes
4
196

APC 900 sx no signs of life.

This was originally posted on APC forums on 8/31/2016


I have two APC 900 SX ups's which seem to be dead.   No lights come on.  No response to on/off button.  Nothing.   Were these blown out in a a surge?   Is there any way to revive them?   The surge only outlets are live, but nothing else responds...

Tags (4)

Accepted Solutions
TTStudio_apc
Crewman
Crewman
0 Likes
0
196

Re: APC 900 sx no signs of life.

This was originally posted on APC forums on 9/2/2016


Thanks.   I've ordered a new battery pair and I'll give it a test.     

See Answer In Context

4 Replies 4
BillP
Administrator Administrator
Administrator
0 Likes
0
196

Re: APC 900 sx no signs of life.

This reply was originally posted by Bill on APC forums on 8/31/2016


Donald,

Please verify the model of the UPS and provide the serial number. The both can be found on a bar code sticker on the back or bottom of the UPS. 

In most cases if the battery outlets do not provide power but the surge outlets do the battery/s are discharged. 

Attachments
TTStudio_apc
Crewman
Crewman
0 Likes
0
196

Re: APC 900 sx no signs of life.

This was originally posted on APC forums on 9/1/2016


Model Number: BX900R

Serial Number: 3B1042X16619 

Thanks

UnexpectedBill_apc
Captain
Captain
0 Likes
0
196

Re: APC 900 sx no signs of life.

This was originally posted on APC forums on 9/2/2016


I think this might be one of the "unique" Back-UPS models that requires a good battery in order to start up. (I seem to remember my very similar looking BK800 wouldn't power up when its batteries were worn out.) Ordinarily that would only apply to the Smart-UPS line, but there are some Back-UPS models that are the same way.

TTStudio_apc
Crewman
Crewman
0 Likes
0
197

Re: APC 900 sx no signs of life.

This was originally posted on APC forums on 9/2/2016


Thanks.   I've ordered a new battery pair and I'll give it a test.