Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80572members
346458posts

AP9640 doesn't display model and won't load properly ion struxureware DCE

Pete_Franco
Cadet
0 Likes
1
64

AP9640 doesn't display model and won't load properly ion struxureware DCE

I replaced a failing NMC in a Smart-UPS 1000 with an AP9640 NMC. The card is not showing the model of the UPS . 

 

I need to get this unit into Struxureware DCE (7.8.1.35) but apparently Struxureware needs more information that the NMC is providing. I can't push new firmware to the UPS because Struxureware doesn't have any data on the device type.

 

This is the view from the web interface2021-12-08_17-49-45.png

 and what I am seeing in Struxureware after I scan for the device

 

2021-12-08_17-58-19.png

 

Anyone experience this or have a solution

Tags (1)
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
47

Re: AP9640 doesn't display model and won't load properly ion struxureware DCE

@Pete_Franco 

 

The screenshot indicates the NMC is not receiving data from the UPS. What are the model and the serial number of the UPS? 

Tags (1)