Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79159members
343629posts

"Untrusted SSL certificate" error - PCNS 3.10 Linux

Solved
vendorbender_apc
Ensign
Ensign
0 Likes
2
472

"Untrusted SSL certificate" error - PCNS 3.10 Linux

This was originally posted on APC forums on 5/26/2015


I am receiving the following error in the Event log when logging into the server running CentOS 6.6 and PowerChute Network Shutdown 3.10 for Linux at [https://[server IP]:6547]:

Connection error because PowerChute received an untrusted SSL certificate from [https://[Mgmt Card IP address:443]. Please enable the option "Accept Untrusted SSL Certificates" on the Network Management Card Connection page or add the certificate to the PowerChute keystore. [More Information]

The only place I can find where the "Accept Untrusted SSL Certificates" setting can be changed is via the "Install Wizard", which is accessible via the web interface once PCNS is installed. Even though I confirmed that this setting was already set as directed, I went ahead and ran the wizard anyway to reset the setting and still receive the same error message. The management card is an AP9619 with latest firmware installed.

Is this a known bug?


Accepted Solutions
vendorbender_apc
Ensign
Ensign
0 Likes
0
472

Re: "Untrusted SSL certificate" error - PCNS 3.10 Linux

This was originally posted on APC forums on 5/26/2015


Wow, I would have thought this would have been made clear during the setup process, or I wouldn't have wasted my time trying to get that to work securely.

Good to know, thanks.

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
472

Re: "Untrusted SSL certificate" error - PCNS 3.10 Linux

This reply was originally posted by Bill on APC forums on 5/26/2015


Phil,

There is no HTTPS solution/support for PowerChute v3.1 registering over HTTPS with an AP9617, AP9618, AP9619. If you required SSL the NMC should be upgraded to a AP9631.

vendorbender_apc
Ensign
Ensign
0 Likes
0
473

Re: "Untrusted SSL certificate" error - PCNS 3.10 Linux

This was originally posted on APC forums on 5/26/2015


Wow, I would have thought this would have been made clear during the setup process, or I wouldn't have wasted my time trying to get that to work securely.

Good to know, thanks.