Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-30 10:31 PM
This was originally posted on APC forums on 4/28/2016
i tried to set up the network shutdown with the 3 up's at first only 1 and 3 could connect so i reset the authentication phrase on all 3 to be admin user phrase
after that i could connect to 2 but not 1 and 3
ive reset the authentication phrase dozens of times to different things, and rebooted the management interface but i cant get it to work.
ive used different browsers, IE AND chrome, still not working. any idea what im doing wrong?
Posted: 2021-06-30 10:31 PM
This was originally posted on APC forums on 5/2/2016
I resolved this by changing the user passphrase to something without spaces in it. as apparently it doesn't like that.
Posted: 2021-06-30 10:31 PM
This reply was originally posted by Bill on APC forums on 4/28/2016
Hi,
Is PowerChute installed and showing no communications with the 2 NMCs and if so on what OS PCNS is installed on? Also, what is the firmware revision running on the NMCs?
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.