Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80828members
346902posts

firmware update for ap9619 from linux

Solved
chappel_apc
Crewman
Crewman
0 Likes
3
168

firmware update for ap9619 from linux

This was originally posted on APC forums on 3/18/2009


I'm trying to find the latest firmware files for an ap9619, which I understand to be a 'network management' card - 'nmcard' (as opposed to the 'web management' card - 'webcard'). I've dug through the ftp site here - ftp://ftp.apcc.com/apc/public/hardware/nmcard/firmware/, but the files in the 'aos' and 'sumx' directories are older than what I've already got - I'm currently running:

Network Management Card AOS v2.5.0
Smart-UPS & Matrix-UPS APP v2.5.1

The 'download shortcuts' link on the apcc site only seems to have the executable all-in-one, which I can read the contents of, but not unpack on my linux (ubuntu 8.1) management station.

Is there somewhere I can download the just the aos and sumx files to do a basic ftp upgrade?

thanks,

ch


Accepted Solutions
chappel_apc
Crewman
Crewman
0 Likes
0
167

Re: firmware update for ap9619 from linux

This was originally posted on APC forums on 3/19/2009


Sweet! renaming the .exe was the missing bit of info - thanks to both of you for the tips.

See Answer In Context

3 Replies 3
voidstar_apc
Janeway
Janeway
0 Likes
0
167

Re: firmware update for ap9619 from linux

This was originally posted on APC forums on 3/19/2009


Rename the executable all-in-one .zip instead of .exe, and then unzip it.

test:~ voidstar$ unzip ~/Downloads/apc_hw02_aos361_sumx358.zip 
Archive:  /Users/voidstar/Downloads/apc_hw02_aos361_sumx358.zip
  inflating: apc_hw02_aos_361.bin    
  inflating: apc_hw02_sumx_358.bin   
  inflating: winftp32.dll            
 extracting: config.txt              
 extracting: iplist.txt              
  inflating: upgrd_util.exe          
  inflating: apc_hw02_aos_202.bin    
 extracting: go.bat                  
Yeah, I wish they didn't assume everyone uses a Windows machine.

BillP
Administrator Administrator
Administrator
0 Likes
0
167

Re: firmware update for ap9619 from linux

This reply was originally posted by Angela on APC forums on 3/19/2009


also, the files on the public FTP site are definitely not the ones you want to use. download the executable for the AP9619 from the software and firmware section of the apc.com if you havent already, AOS 3.6.1 and SUMX 3.5.8, and then you can unzip it has voidstar mentioned and [follow these directions|http://nam-en.apc.com/cgi-bin/nam_en.cfg/php/enduser/std_adp.php?p_faqid=768]

hope that helps!

chappel_apc
Crewman
Crewman
0 Likes
0
168

Re: firmware update for ap9619 from linux

This was originally posted on APC forums on 3/19/2009


Sweet! renaming the .exe was the missing bit of info - thanks to both of you for the tips.