Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-07-01 12:33 AM
This was originally posted on APC forums on 8/11/2011
using powerchute 3 and the only two runtime options appear to be:
1. to shutdown the computer when it is on battery after 1-5 minutes. or
2. shutdown computer when battery runtime is 5-8 minutes.
This is a poorly phrased or bad option. If the runtime is only 8 minutes and I want to leave it on as long as possible, it seems like I can't select the option that says "keep on as long as possible" as that option only goes down to 5 minutes. What if I want 2 minutes etc? As is, I'd get 3 minutes of runtime and then it would shutdown it would seem. Is there a spot to edit that manually.
I might assume that if I select the other option "preserve battery power" and select shutdown after 5 minutes of battery use, that the battery would actually run the whole 5 minutes vs 3 in the other method.
Posted: 2021-07-01 12:33 AM
This reply was originally posted by Jonathan on APC forums on 8/17/2011
Hi Max,
If you are using a Microsoft Based Operating System, you can take a look at the Native UPS software that comes with it and see if that suits your need. Unfortunately when it comes to our software, those values are the default. I think I have encountered a thread before wherein the customer made some changes on their registry. I wouldn't recommend doing this if you are not familiar with registries for it can cause unwanted issues such as corruption of the Operating System.
Posted: 2021-07-01 12:33 AM
This reply was originally posted by Jonathan on APC forums on 8/17/2011
Hi Max,
If you are using a Microsoft Based Operating System, you can take a look at the Native UPS software that comes with it and see if that suits your need. Unfortunately when it comes to our software, those values are the default. I think I have encountered a thread before wherein the customer made some changes on their registry. I wouldn't recommend doing this if you are not familiar with registries for it can cause unwanted issues such as corruption of the Operating System.
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.