Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79300members
343972posts

change runtime

Solved
1max4820_apc
Cadet
0 Likes
1
65

change runtime

This was originally posted on APC forums on 8/11/2011


using powerchute 3 and the only two runtime options appear to be:
1. to shutdown the computer when it is on battery after 1-5 minutes. or
2. shutdown computer when battery runtime is 5-8 minutes.

This is a poorly phrased or bad option. If the runtime is only 8 minutes and I want to leave it on as long as possible, it seems like I can't select the option that says "keep on as long as possible" as that option only goes down to 5 minutes. What if I want 2 minutes etc? As is, I'd get 3 minutes of runtime and then it would shutdown it would seem. Is there a spot to edit that manually.

I might assume that if I select the other option "preserve battery power" and select shutdown after 5 minutes of battery use, that the battery would actually run the whole 5 minutes vs 3 in the other method.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
65

Re: change runtime

This reply was originally posted by Jonathan on APC forums on 8/17/2011


Hi Max,

If you are using a Microsoft Based Operating System, you can take a look at the Native UPS software that comes with it and see if that suits your need. Unfortunately when it comes to our software, those values are the default. I think I have encountered a thread before wherein the customer made some changes on their registry. I wouldn't recommend doing this if you are not familiar with registries for it can cause unwanted issues such as corruption of the Operating System.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
66

Re: change runtime

This reply was originally posted by Jonathan on APC forums on 8/17/2011


Hi Max,

If you are using a Microsoft Based Operating System, you can take a look at the Native UPS software that comes with it and see if that suits your need. Unfortunately when it comes to our software, those values are the default. I think I have encountered a thread before wherein the customer made some changes on their registry. I wouldn't recommend doing this if you are not familiar with registries for it can cause unwanted issues such as corruption of the Operating System.